Position_Actual_Internal_Value
| Index.Sub | 6063.0H |
| Data Type | Integer32 |
| Access | Read Only |
| PDO Mappable | No |
| Unit | Increments |
|
Range |
-2147483648 to 2147483647 |
| Default Value | 0 |
| Store Supported | No |
| Description | This object provides the position actual value of the Feedback Sensor or Motor (with Sensor_selection_code object is possible to select the motor or encoder reference). |
|
Notes |
-- |